Forums

Reply
DF1 Devotee
rabbit
Posts: 5
Registered: 07-03-2008
0

enpac 2500 SD card

I am having a very dificult time finding the SD cards specified in the Enpac manual.  I have tried a Sandisk card and received a error message - Errors were detected during the formatting of "SD Card". Do I have to have the specified cards or is there some other step I need to take to get the any SD card to work?

This one is so good … we couldn't think of a title good enough!
fuzzy_logic
Posts: 2,825
Registered: 06-26-2008
0

Re: enpac 2500 SD card

You may find some informations about SD card inside the following technotes:

 

Aid 42456 - Aid 53937

 

- fuzzy logic

Please remember to close your thread, using the Accept as Solution button over the answer that solved it... and click the Star ( ) under the user avatar to assign Kudos to those who provided help. Thanks... :smileywink:
DF1 Devotee
rabbit
Posts: 5
Registered: 07-03-2008
0

Re: enpac 2500 SD card

Ok I got a Edge 1 GB SD memory card.  When installed in the EnPac ther was no request to format or initialize. The card is being seen by the Enpac in the about window. The folowing is all the infomation on the Enpac. Enpac 2500 data Collector; Unit ID: 0000-02ec-fec7; Firmware Version: 3.00; (Two Channel); (With Offroute); Internal Disk 100% Free (27.1 MB total); SD Card 100% Free (955.1 MB total). The problem is I can load a list to the internal memory card just fine.  I initialize the Enpac and switch to the SD card and try and load the same list and I get an Emonitor Factory error "Cannot load XXXXXX to Enpac 2500 USB. Load file corrupted." 
This one is so good … we couldn't think of a title good enough!
fuzzy_logic
Posts: 2,825
Registered: 06-26-2008

Re: enpac 2500 SD card

Well, apologize first as I'm not an expert of this, just trying to help... :smileysad:

 

Here a *collection* of technotes I've found, hope you will find something useful there...

 

Aid 39492 - Aid 37900 - Aid 47245 - Aid 55245

 

- fuzzy logic

Please remember to close your thread, using the Accept as Solution button over the answer that solved it... and click the Star ( ) under the user avatar to assign Kudos to those who provided help. Thanks... :smileywink: