Forums

Reply
New Member
Wailung
Posts: 2
Registered: 07-15-2009
0

Allen Bradley breakers and motor starter

I am working on some short circuit study but I can't find any information on the following items:

 

G100 series breaker 10A

G500 series breaker 50A

G150 series breaker 15A

Manual motor starter, 140-MN-0400

This one is so good … we couldn't think of a title good enough!
fuzzy_logic
Posts: 2,825
Registered: 06-26-2008

Re: Allen Bradley breakers and motor starter

[ Edited ]

If you're searching infos about 1492-CB, try to take a look to the following links:

 

http://www.ab.com/en/epub/catalogs/12768/229240/471158/1213079/3170943/index.html

http://www.ab.com/en/epub/catalogs/12768/229240/471158/1213079/3170943/tab5.html

http://192.94.123.20/idc/groups/literature/documents/td/1492-td011_-en-p.pdf

 

About 140-MN, see Aid 31534

 

Considering the obsolescence of certain items, it is difficult to find out those infos, that are available on old Catalogs...I suggest to call your local Rockwell Automation representative to get more informations.

 

Hope this helps…

 

- fuzzy logic

Message Edited by fuzzy logic on 07-16-2009 08:29 AM
Please remember to close your thread, using the Accept as Solution button over the answer that solved it... and click the Star ( ) under the user avatar to assign Kudos to those who provided help. Thanks... :smileywink:
New Member
Wailung
Posts: 2
Registered: 07-15-2009
0

Re: Allen Bradley breakers and motor starter

Thanks a lot!