Forums

Reply
New Member
Titan AE
Posts: 1
Registered: 10-06-2009
0

800H Standard, Push-To-Test question

Helo,

 

I have a question about Pilot Lights. 

 

I installed a few Pilot Lights that are incandescent type model #s:

800H-QR24R, 800H-QR24A, 800H-QR24G & 800H-QR10G.

 

What I need is an LED type lights. Is the possible to change the incandescent type pilots light to LED

type by swapping the illumination option without changing the whole unit?

 

The LED model #s are:

800H-QRH24R, 800H-QRH24A, 800H-QRH24G & 800H-QRH10G.

 

Thanks.

DF1 Devotee
pv550
Posts: 5
Registered: 01-29-2009
0

Re: 800H Standard, Push-To-Test question

I don't see a problem replacing incandescent with LED as long as LED color matches lens with the exception for amber LED requires white lens.

 

Green LED 800T-N319G 24vac/dc

 

Green LED 800T-N169G 130vac/dc

 

Red LED 800T-N319R 24vac/dc

 

Amber LED 800T-N319A 24vdc/ac