- Subscribe to RSS Feed
- Mark Topic as New
- Mark Topic as Read
- Float this Topic to the Top
- Bookmark
- Subscribe
- Printer Friendly Page
Ultra 3000 2098-dsd-3 0 drive
- Mark as New
- Bookmark
- Subscribe
- Subscribe to RSS Feed
- Highlight
- Email to a Friend
- Report Inappropriate Content
08-20-2009 07:48 PM
how can i start a motor F-4050-Q-H00AA without connecting any inputs. Also,can some email me the cable number or wire diagram for this drive: where inputs are located etc. oral.golaub@gmail.com
Re: Ultra 3000 2098-dsd-3 0 drive
- Mark as New
- Bookmark
- Subscribe
- Subscribe to RSS Feed
- Highlight
- Email to a Friend
- Report Inappropriate Content
09-10-2009 04:26 PM
As far as a wiring diagram, check the user installation manual 2098-IN003. It is available from the literature library found at www.ab.com
As far as starting the motor on power up, would need the compete part number of the drive. It this configured for indexing? If so, there is an auto indexing mode that when the drive is powered up and the enable input goes high, it starts its indexing cycle. Check article 44622 in the Knowledge Base.