Forums

Reply
New Member
cgman
Posts: 1
Registered: 10-07-2009
0

SERCOS Card inquiry

Is the Sercos card supposed to be installed where the Processor is at? or can it be placed in the Remote rack?

This one is so good … we couldn't think of a title good enough!
fuzzy_logic
Posts: 2,825
Registered: 06-26-2008

Re: SERCOS Card inquiry

Motion Modules CANNOT be located in remote chassis

 

See Aid 41712 for details.

 

- fuzzy logic

Please remember to close your thread, using the Accept as Solution button over the answer that solved it... and click the Star ( ) under the user avatar to assign Kudos to those who provided help. Thanks... :smileywink: