Forums

Reply
New Member
oral
Posts: 1
Registered: 08-16-2009
0

Ultra 3000 2098-dsd-30 drive

how can i start a motor F-4050-Q-H00AA without connecting any inputs. Also,can some email me the cable number or wire diagram for this drive: where inputs are located etc. oral.golaub@gmail.com

FactoryTalk Fabulous
deekster
Posts: 66
Registered: 06-06-2008
0

Re: Ultra 3000 2098-dsd-30 drive

As far as a wiring diagram, check the user installation manual 2098-IN003.  It is available from the literature library found at www.ab.com

 

As far as starting the motor on power up, would need the compete part number of the drive.  It this configured for indexing?  If so, there is an auto indexing mode that when the drive is powered up and the enable input goes high, it starts its indexing cycle.  Check article 44622 in the Knowledge Base.