- Subscribe to RSS Feed
- Mark Topic as New
- Mark Topic as Read
- Float this Topic to the Top
- Bookmark
- Subscribe
- Printer Friendly Page
1394 turbo system losing program
- Mark as New
- Bookmark
- Subscribe
- Subscribe to RSS Feed
- Highlight
- Email to a Friend
- Report Inappropriate Content
10-28-2009 03:55 PM
Re: 1394 turbo system losing program
- Mark as New
- Bookmark
- Subscribe
- Subscribe to RSS Feed
- Highlight
- Email to a Friend
- Report Inappropriate Content
10-28-2009 04:09 PM
What parameters in particular are lost - all of them or just some?
Could it be that these are being written to by an external device and the 1394 not losing the data?
If its the battery, then the data must be stored in a different type of memory from the application program, otherwise you would lose that as well.
The following is from the KB on the subject (Ans ID 27691). The following isn't what you want to read - so need to be sure its the battery thats causing your issues.
BATRAM KEY FEATURES
10 years minimum data retention in the absence of external power
Data is automatically protected during power loss
Unlimited write cycles
Low-power CMOS
Lithium energy source is electrically disconnected to retain freshness until power is applied for the first time
Summary: The battery back up RAM (batram) for the 1394 GMC & 1394 GMC Turbo is NOT field replaceable, the unit MUST be sent in for repair. The batram is a self-contained lithium energy source and control circuitry.
Catalog Number: 1394 GMC;1394 GMC Turbo
DocFullNum: G73448994
Re: 1394 turbo system losing program
- Mark as New
- Bookmark
- Subscribe
- Subscribe to RSS Feed
- Highlight
- Email to a Friend
- Report Inappropriate Content
10-28-2009 04:22 PM
On Off Off Solid - Memory fault - Setup or program checksum errorb - Re-Download the GML diagram with the setups - Reset the controller.
Re: 1394 turbo system losing program
- Mark as New
- Bookmark
- Subscribe
- Subscribe to RSS Feed
- Highlight
- Email to a Friend
- Report Inappropriate Content
10-28-2009 04:31 PM
Sounds like you've lost everything when this happens.
Maybe its time for that repair as mentioned in the tech note.
Re: 1394 turbo system losing program
- Mark as New
- Bookmark
- Subscribe
- Subscribe to RSS Feed
- Highlight
- Email to a Friend
- Report Inappropriate Content
10-28-2009 04:59 PM