Forums

Reply
AJZ
DF1 Devotee
AJZ
Posts: 8
Registered: 07-23-2008
0

Lost all axisname.AbsoluteReferenceStatus bits

A four axis 1769-L43 with SERCOS based has been working fine for almost a year. All motors are MPL with multi-turn absolute encoders Then one morning all axisname.AbsoluteReferenceStatus bits were off. The encoders were still reading the correct value. Just moved the axis to the absolute home position using motion direct command and performed a MAH using motion direct commands.

 

WHat can cause the system to loose all  axisname.AbsoluteReferenceStatus bits at the same time?

This one is so good … we couldn't think of a title good enough!
fuzzy_logic
Posts: 2,825
Registered: 06-26-2008
0

Re: Lost all axisname.AbsoluteReferenceStatus bits

[ Edited ]

Just trying to help, as I'm not an expert on this :smileytongue:

 

Aid 47351 reports the cases where the bit is either set or reset.

 

After that, you may consider three cases where a problem could be in the code:

 

1. MAH (Motion Axis Home) repeated more than once in code, thus resetting the absolute position reference.
2. MRP (Motion Redefine Position) repeated more than once in code, thus resetting the absolute position reference.
3. Changing from Linear to Rotary mode within the code.

 

Double check if you're in one of these cases, then take the appropriate actions to solve.

 

If you are not in those cases, please post again so that other folks here will have the possibility to help you more.... :smileywink:

 

- fuzzy logic

Please remember to close your thread, using the Accept as Solution button over the answer that solved it... and click the Star ( ) under the user avatar to assign Kudos to those who provided help. Thanks... :smileywink:
AJZ
DF1 Devotee
AJZ
Posts: 8
Registered: 07-23-2008
0

Re: Lost all axisname.AbsoluteReferenceStatus bits

The drives are Kinetix6000.

There are no MAH or MRP instructions in the code. I use 'motion direct commands' to set the absolute position reference.

DF1 Devotee
sdfs
Posts: 2
Registered: 08-20-2008
0

Re: Lost all axisname.AbsoluteReferenceStatus bits

In the event of an E73 or E76 fault when control power is removed from the system, the absolute reference bit will be cleared on AM modules. Note that these faults are rare and are typically caused by hardware failures or bent pins on the power rail.