Forums

Reply
New Member
Robin Ellwood
Posts: 1
Registered: 06-26-2009
0

Crossworks Error

Hi

 

Did a cross reference on Sic Part number IM1204BPSZW1 and got two different answers

Depending on if I used dashes in the part number.

 

IM12-04BPS-ZW1 gave me a 872C-D4NP12-A2

IM1204BPSZW1   gave me a 872C-M4NP12-A2

 

I had no problem with this as I confirmed the application with the customer and used the Extended Range unit "M4but I though it should be corrected as it could cause issues with others.

 

I am not sure if this is the correct procedure to correct this but I thought it would be a good start.

 

 

Thanks

 

Robin

New Member
mocampoRA
Posts: 2
Registered: 06-08-2009
0

Re: Crossworks Error

Hello Robin,

 

Thank you for informing us on this CrossWorks error.  The error has been fixed and the corrected information will be available to all CrossWorks users after the July 9th Current Update. 

 

Thanks,
Marcelo